ROHM Wins Silver Class in Overall Category of SUSTAINA ESG AWARDS 2018!

  • 2018-10-30
  • Governance

ROHM was selected as Silver Class of Sustaina ESG Awards 2018 by SUSTAINA, a company that provides an online platform using AI (Artificial Intelligence) technology to evaluate overall ESG (Environmental, Social, Governance) performances of more than 4,000 companies based on the International Standard of Social Responsibility - "ISO26000".

The purpose of this 「SUSTAINA ESG AWARDS」 is to raise awareness and encourage more companies to be more actively involved in promoting CSR/ESG activities by rewarding selected leading companies to serve as role models.

In Overall Category, 100 companies with highest total scores are selected as the "ESG Management Leading Companies". The top 20 companies are selected as Gold Class, 30 companies are Silver Class, and the rest 50 companies are selected as Bronze Class. In this year's reward, ROHM was selected as Silver Class as one of the top 30 companies that has implemented excellent CSR/ESG Mangement and initiatives.

From now on, the ROHM Group will continue to put efforts in disclosing our ESG information to the public and carrying out more CSR activities, in order to strengthen the trust relationship with our stakeholders.

Back to Index